FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
2 weeks ago - last edited 2 weeks ago
Hello!
I am currently using InfluxDB for data storage. I have an SD card mounted as a memory extension, and in the InfluxDB configuration file (influxdb/config.yaml), I have specified the following paths:
However, after some time of storing data, I noticed that my ctrlX internal storage became full, while the memory card remained empty:
Once I deleted the respective InfluxDB bucket, the internal memory returned to normal:
This indicates that the InfluxDB data is being stored on the internal memory instead of the memory card. Is this the expected behavior?
Thanks in advance! 😊
2 weeks ago - last edited 2 weeks ago
Hi @star_board
your yaml should look like this:
Which version are you using?
Regards
CodeCaptain
2 weeks ago - last edited 2 weeks ago
As suggested by @TheCodeCaptain , please provide your configuration: apps and versions and which OS version you are using
2 weeks ago
Does this means that I can't storage data on the SD card if I have it mounted as removable medium on the ctrlX?
2 weeks ago
I am currently using Telegraf to write metrics to the InfluxDB App.
I am using LTS Release 2.6:
2 weeks ago
Hello,
I need also the "system apps" version if possible if you can do a system report would be perfect.
It is definitely possible, we have many running since a lot of time collecting many data. Follow this guide and use the memory as "Removable Media" for now, we investigate the root cause of your setup here there is the guide:
With your setup you can collect also realtime data:
2 weeks ago
Here are all the applications installed on the device:
a week ago
I have followed the guide and set the memory as "Removable Media," but I am not sure if data is being saved to the SD card. How can I verify this?
a week ago
a week ago - last edited a week ago
Yes!
Is there a way to actually verify where data is beeing written to?
a week ago
a week ago - last edited a week ago
Yes, that's the name!
a week ago
a week ago - last edited a week ago
Just to clarify, as of now, there isn't a method to check if data is truly being saved to the SD card?
The alternatives I found were:
Tuesday
Hello,
The problem is strictly related to the device used toghether with "EXTENSION OF INTERNAL MEMORY". Any other usage is not affected.
We are working on a fix. I update you as soon as we have a schedule for fix 😁