FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
01-10-2024 01:26 PM
Which app version should we use for ctrlX OS version >= 2.xy?
Should we use the actual available version 118 with core20?
Solved! Go to Solution.
01-10-2024 02:05 PM
Hi @LunatiX
unfortunately there is no IDE App Version 2 at the moment. The latest Version is IDE-V-0118.37.app. You can use this version with a little workaround with ctrlX OS V2 if you also install the core20 app.
Best regards,
Nick
02-22-2024 11:38 AM
Hi @nickH, I have installed the IDE App with OS V2.
but I got this error:
Do you think it's due to the incompatibility of the system apps?
02-22-2024 02:02 PM
Hi @redford
I would guess the error is in your script. Or that the dependencies of your script are not available, at least this is what the error indicates.
Best regards,
Nick
02-22-2024 02:42 PM
Hi @nickH
It is just a test program, to check whether the app works. It consists:
One Axis
Initialized in IDE
The axis should move.
If I click "start", the error appears.
02-23-2024 10:16 AM
Ok. I can reproduce the same error. So the workaround I mentioned does not work. You would have to wait for the version 2 to be released.
Thanks for mentioning the issue.