Changing the state of the master ETHERCAT from Node-RED

Changing the state of the master ETHERCAT from Node-RED

Good morning, I have a problem changing the state of the ETHERCAT master from INIT to OP in Node-RED. I was able to update its state directly from the CORE by writing a JSON with the following structure: {"request": {"newState": "op"}} and by using HTTP went OK too, but when try to modify it from Node-RED, it gives me the following error: CtrlxProblemError: DL_TYPE_MISMATCH. I have tried the methods WRITE and CREATE  in the data layer request node, at the path fieldbuses/ethercat/master/instances/ethercatmaster/admin/fieldbus_status/master_state, but both give me the same error. The JSON structure sent by the payload is the same as the one I write at the CORE. I have attached several photos of how everything is configured. How can I modify this value with data layer request node?  Thank you so much!

what I recived from debugswhat I recived from debugs

how i did the connectionhow i did the connectionthe structure from the JSONthe structure from the JSON

 

 

2 REPLIES 2

CodeShepherd
Community Moderator
Community Moderator

A "Write" must be used and the "Payload" switched to "value + type (json)". Then send following payload:

 

msg.payload ={"type": "object", "value": {"request": {"newState": "op"}} }
return msg;

 

See all my standard examples on github. Or see also this thread for another complex example.

Thank you so much, It works properly!!

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist