06-16-2023 02:26 PM
Hi,
is it possible to shadow a ethercat slave that is not powered. So ethercat can go to OP. And after i power on the slave the ethercat working on. Actually i will get the problem that i have an topologie missmatch. And the I/Os from the Ethercat and also the Datalayer not update the IOs. All my mapped DI are false. Without so DIs i can not quit the safety and so powered this missing ethercat slave
I configured that the ethermaster like, that slaves have not to reach master state. But i get no I/Os from the operating clamps but they have state OP
Solved! Go to Solution.
06-16-2023 03:45 PM
You not only need the setting for slaves do not reach EtherCat master state but also use different sync units for the data transmission. See this thread.