11-12-2021 02:29 PM
Hello,
does still current (RM21.07) IO Engineering software support some kind automatic detection of IO plugged behind the coupler? It can be only manually added. Correct me in case I am wrong
Thank you!
Solved! Go to Solution.
11-15-2021 07:50 AM
This is a topic of the EtherCat functionality and the S20 bus couplers. You cannot scan "throug" devices, when they are not known in the bus. This will be different in the ctrlX IOs because there each IO is an own slave.
You have to scan once the coupler then download the EtherCat configuration to the ctrlX CORE. Afterwards simply scan again and the sub modules will be found (if you have problem at the second scan try to switch EtherCat state to Safe-Op or Pre-Op).