FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
02-09-2022 02:24 PM
Hello
I am trying to set up an analog module for 4-20 mA, S20-AI-8 with a S20-EC-BK and a ctrlX CORE. I have copied the example from the library but I always get an error when I am executing the FB.
I have the analog module on slot 1 and the ethercat bus coupler has address 1001. Ethercat name is "ethercatmaster".
The error code I get is DEVICE_ERROR and ErrorIdent is CXA_TABLE,
Additional 1 0x80000000
Additional 2 0x00000000
I am using ctrlX WORKS 1.12.2
Are there some prerequisites that I have missed?
I have license for PLC basic and standard and Ethercat license.
Solved! Go to Solution.
02-10-2022 09:40 AM
Hello,
there is a bug in the CXA_Ethercatmaster Lib. Downgrade to 1.10.1.0 or update the lib to at least 1.12.2.0. This can be easily done via Placeholder in library manager.
In ctrlX WORKS 1.12.4 the latest CXA_Ethercatmaster lib should be included.
02-11-2022 06:47 AM
Hello
Thanks, it worked when I switched to EthercatMaster lib verion 1.12.3.0