FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
07-18-2023 03:03 PM
Hello everybody,
I am trying to configure an S20 EtherCAT buscoupler as DC-Synchronous on a ctrlX Core as in the image:
When I download the configuration the EtherCAT Master (the ctrlX Core) goes in OP mode while the EtherCAT slave (the Buscoupler) remains in Pre-OP mode with the error "0x0028: SynchMode not supported" as the image:
Why this happens? I would experct that if the DC-Synchronous mode is selectable (it cames from the ESI-file) the DC Mode is supported.
Am I missing something or some configurations?
Best regards
Andrea Toffalori
Solved! Go to Solution.
07-20-2023 09:41 AM
Hello Andrea Toffalori,
it's because none of the used modules is supporting sync. It will work when you plug a module which supports sync, like S20-AO-4 or S20-INC-2.
07-21-2023 12:30 PM
Hello,
do you know all the modules that support the DC synch mode? Or do you have to look at the Data Sheet of every single I/O module?