FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
11-29-2023 12:18 PM
The EtherCAT master app is limited by:
Is there any way to check the amount of input/output data in an offline configuration?
Is it known when these limits will be increased for the X7?
Solved! Go to Solution.
11-29-2023 02:04 PM - edited 11-29-2023 03:27 PM
You can check all licensed software metrics like utilized IO data via the corresponding tab in the device data in the ctrlX PLC Engineering online and offline:
The current features can be found in our online documentation "EtherCAT Master – Features".
The numbers for ctrlX CORE X3 stay the same in the future. For ctrlX CORE X7 the input and output data combined was increased to 10kB from version 2.02 as the sum is the value that counts. The number of slaves will be increased next year.
11-29-2023 02:31 PM
Thanks CodeShepherd.
But the documentation distincts input and output data. The IO Data metrics show the combined in- and outputs?
11-29-2023 03:24 PM - edited 11-29-2023 03:28 PM
Like tried to mentioned above from version 2.02 it will be mentioned as combined in the documentation as the sum is the counting value. I edited my post to better point this out.