05-29-2023 03:05 AM
Can S20 Bus Coupler (Ethernet IP) connect with ctrlX Digital/Analog Input/Output modules?
And what are the requirements on the communication and connection?
Is there a plan on ctrlX Ethernet IP bus coupler?
Solved! Go to Solution.
05-30-2023 07:03 AM
Hallo,
no this is not possible!
Regards
06-12-2023 10:47 AM
Like mentioned by @Sozu it is not possible. This is because the ctrlX IOs can only be used via Ethercat fieldbus.