10-21-2022 01:57 AM
Hello,
ctrlX IO engineeing/ EtherCat Master is not able to recognize the EK1100 bus coupler , XML are installed in Device repository. What could be the reason ?
Core version is 1.12
we tried to add the device manually without success.
Solved! Go to Solution.
10-21-2022 07:47 AM - edited 10-21-2022 09:56 AM
It still looks like only the IO submodules are installed but not the coupler itself. Could you add a screenshot of your device repository with the coupler and at best share the device description files you used.
EDIT: In your screenshot you can see that the coupler is from company "NUM AG" so you also have to get the device description from them.
10-27-2022 01:44 AM
Hi ,
Bus coupler delivered by beckhoff was not programmed correctly, customer had some support and wasable to reflash the module with the proper ID. Thanks !