cancel
Showing results for 
Search instead for 
Did you mean: 

oscilloscope function / IOT

oscilloscope function / IOT

Is it possible to read a recording from the oscilloscope in the drive via an IOT gateway (also from external devices! Not necessarily Core) as CSV, XML, etc.? In my case, ctrlX D is connected to an S7 via ProfiNet.

5 REPLIES 5

MauroRiboniMX
Contributor

Hello, 

Of course, you have to use a ctrlX CORE https://developer.community.boschrexroth.com/t5/Store-and-How-to/IIoT-Collect-Data-from-ctrlX-Drive-...

Note that this guide has been done with the old version of the "Drive connect" app. So can be that somethingshould be adapted 😁

  • Hello Mauro,
    That sounds good at first.

    - Can't I just read out individual parameters there? I want to transfer an entire curve from the oscilloscope as a table (CSV, XML, etc.)?

    - Is there also a possibility without our core and without the Drive Connect app. The customer has an external IOT gateway, not a core from us? Otherwise he would have to use our core in addition to his gateway.

 

You can, via parameters, activate the oscilloscope and get the data. soo yes, just parameters but those are able to get gata from the oscilloscope. 

 

this is not an answer of my questions...

Then probably you have to reframe the question again. 

Current answer is, yes you can read out the measurement by reading out the parameter that are including the recorded data.

You could also use the EAL (Easy Automation Library) for direct communication between an external application and an ctrlX DRIVE, via an proprietary protocol.

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist