FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
07-15-2024 04:49 PM
we should operate ctrlX Drives (XCS2-W0090 / R914511786) at highest railway station in tibet at 5200 m above sealevel. the max in our manual is 4000 m with derating.
- is it possible to use the drives in this altitude and what are the rules and conditions (Deratings) to make it possible?
- what is the risk? ... and of course it has to take the customer by himself.
Solved! Go to Solution.
07-18-2024 06:27 PM
This is out of the specifications and not possible. One has to create ambient conditions (temperature, outside pressure, etc.) which are equivalent to 4000m height.