FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
01-12-2021 12:09 PM
Hello Collegue,
we're developing a proposal for MT rotary transfer machine with 19 Spindels and 46Axes.
The point is the filter, two questions:
- Is there the possibility to exeed the limitation of 800nF related to HNF01.1C-F240-E0150?
- What problem/defect can occour if we use a filter with a relevant gap in Y capacitance versus all drives? (filter 800nF <> drives+Power supply 1500nF)
Any suggest for application with several drives?
Thank you
PL
Solved! Go to Solution.
01-13-2021 10:54 AM
With the hardware versions coming end of March/beginning of April 2021 the former mains filter of IndraDrive can be used in conjunction with ctrlX DRIVE. Then a higher amount of cable lengths and Y capacitances can be established.
For exact details get in contact with the proper people in Drive Support via Email exchanging the exact type codes and technical data of the components suggested to this machine.
01-14-2021 02:33 PM
Hello Uve,
ok, thank you very much.