07-05-2022 09:47 AM
Hello,
with AXS0304 it was possible to enable the drive by writing P-0-4028 direct from TechFunc with direct variables. With AXS0308.01 it is only possible to write P-0-4028 if the parameter is visible online in the parameter editor or the parameter group. If the editor or the group are not opend the drive goes back from Af to Ab independently after 2 seconds.
My question: Is this behaviour intended? Is it not allowed to write P-0-4028 with direct variables?
Which other possibility we would have to enable the drive?
Thanks
Solved! Go to Solution.
07-08-2022 03:43 PM
Hello.
We habe made some tests, but for us it isn´t possible to reproduze this behaivor.
We check this together in the next days.
07-11-2022 10:11 AM
09-14-2022 09:54 AM
To write P-0-4028 via DV is possible, but must be permanent and cyclical.