cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Profinet parameter channel

Profinet parameter channel

POUL
Established Member

Hi

 

Is the prameter channel running as a part of the Profinet on CtrlX drive?

If yes - is it compatibel with IndraDrive?

 

3 REPLIES 3

CodeWasi
Occasional Contributor

Hello

the parameter-channel integrated in the cyclic communcation to provide acyclic parameter services is not available on the ctrlXDrive.

Bye

I already saw this, when we were preparing the first tests with the ctrlX Drive in profinet.

Well, it really is a small disaster... The parameter channel allowed changes to certain parameters, such as mechanical ratios, which are not available in the process data... And not only the parameter channel has disappeared.. .. keep looking to find more things and some differences.

Bye

Gruffi
Long-established Member

acyclic access via 
- SIP TCP/IP protocol, details https://docs.automation.boschrexroth.com/doc/699034151/s-ip-protocol/latest/en/
- Profinet Read / Write Record with the help of the Alias Parameters is possible with at least AXS-V-0316 or newer (AXS-V-0314 support access to I&M only)

Example Siemens PLC available, SIP function works with ctrlX Drive and IndraDrive.

https://www.boschrexroth.com/de/de/search.html?q=tia&lang=DE&origin=header&num=10&s=download

Gruffi_1-1678112956578.png

 

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist