FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
07-24-2024 02:41 PM
Hello Team,
One of our customer has a problem with Siemens Safety PLC and our CtrlX Drive.
When they bootup the whole machine (Power OFF the whole machine and power back ON) the CtrlX drive usually bootup very fast and waits for the Siemens Master and safety PLC to Bootup, but after the Siemens Master and Safety PLC is booted up, the CtrlX drive doesn't acknowledge it, even after sending enable command from the master and also from safety PLC, The drive keeps in emergency stop state.
But when we boot the Siemens Master and safety PLC first and then the CtrlX Drive, then there is no problem. Could you please help me with a solution for this?
Customer is using FWA-XD1-AXS-V-0402N-NN-03. XCS2
Thank you
Solved! Go to Solution.
07-25-2024 10:28 AM
Hello,
to reproduce this issue please provide a parameter file (all parameters).
Best regards
08-02-2024 05:47 PM
2 weeks ago
Hello, the solution should be the reinitialization function on PLC side, see screenshot.