cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

MS2N hybride cable for EC interface on ctrlX Drive

MS2N hybride cable for EC interface on ctrlX Drive

Pinball_NL
New Contributor

Here a special question. 

We have this RH2 cables for the one cable solution between MS2N motor and HCS01 Drive. (Encoder is 15pole sub-D)

Then we have this RHB2 cable for MS2N and ctrlX drive (Encoder is this small black connector)

Do we also have a Hybrid cable for MS2N on ctrlX drive to connect to the EC encoder interface. (Encoder is 15 pole Sub-D)

I need this back connector for the power and Sub-D for the encoder.  Do we have that, or should I order the RH2cable with a separate black power connection ? And to be sure, the black encoder cable should be long enough to reacht the EC encoder interface on the Drive, but as I can see with Indradrive this should be fine. 

 

1 REPLY 1

Drives_Uwe
Community Moderator
Community Moderator

MS2N motors with AcuroLink encoder have to be plugged into XG20 at ctrlX DRIVE. The multi-encoder connection at XG21 is not suitable.

Therefor the cable must be looking like RHB2.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist