Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

remotely connect

remotely connect

JHU1XI1
Long-established Member

Hello,

The core is already connected to the router. How to remotely connect to the core through works.

3 REPLIES 3

nickH
Community Moderator
Community Moderator

Hi, 

first make sure your PC is in the same network as your ctrlX CORE (look at the ip settings on your PC). Then you can connect to the ctrlX COREs webpage by simply inserting the ip-address of the ctrlX CORE into a webbrowser. 

In ctrlX WORKS you are able to see all the controls, which are present in your local network. (In addition ctrlX WORKS also gives you the possibility to create virtual controls.)

Bet regards, 

Nick

 

 

JHU1XI1
Long-established Member

Hello Nick,

Thank you for your advice.

It can be connected normally on the same local area network, but currently the core and engineering technicians are in different places and need to access the core through an external network. Currently, the core cannot be searched. Is there any setting in the core that will prevent external network access?

2023-05-26_13h57_50.png

nickH
Community Moderator
Community Moderator

If you are connected to network B in the same subnet as the ctrlX CORE (via a vpn), then there is nothing preventing you to connect to the ctrlX CORE via your browser. At least from the ctrlX side. Just type in the ip-address of the ctrlX CORE in your browser and connect. 

That you are not able to see the ctrlX CORE automatically in ctrlX WORKS can sometimes be the case, depending on the networks firewall and router settings. 
But in this case you can still add a link to this ctrlX CORE to ctrlX WORKS via the "+"-button. See also the manual of ctrlX WORKS. 

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist