03-12-2024 11:53 AM
Hello,
1) can I encrypt the setup file when created using the password typed on the UI or set via REST Post request?
I would like to have an encrypted setup file, which I upload and apply via REST.
2) What is the function of the password typed in the UI?
It seems when setup is created and password is set, the password is not required for applying of that setup file.
Thanks,
Venzi
Solved! Go to Solution.
03-15-2024 01:38 PM
Hi @Venzi_
I think the current implementation of the password does not make sense. I forwarded your issue internally. I will let you know when I got news for you.
Thanks for reporting and best regards,
Nick
04-11-2024 02:05 PM
As an update to this topic, here the current state: