FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
09-02-2023 04:16 PM
Hi everyone,
In order to deploy a docker image on Container Engine, I accessed the virtual-ctrlX-core via SSH with "rexroot" system user.
But when I want to run "docker compose" I get the error "command not found" as if docker was not installed on the linux environment of my virtual-ctrlx-core…
For info, my goal is to deploy some docker instances like in this video tutorial : Deploy-Docker-Image-to-Container-Engine-App
Thanks in advance for any input …
Solved! Go to Solution.
09-04-2023 05:50 PM
Hello,
You have to create an app with inside the image and the docker compose. SSH is just for debugging and not open in production devices.
09-06-2023 03:32 PM
Hello Autem,
I was the author of the video and I'm sorry if this point wasn't clear. The Container Engine application automatically creates instances from your container images based on the specification provided in the docker-compose file you package with your image snap. You can also manually create and destroy containers using the Container Engine menu in the ctrlX Web UI.
10-12-2023 07:16 AM
Moved to own topic.