FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
11-22-2022 09:34 AM
Are there any recomondations for time settings?
Solved! Go to Solution.
06-20-2022 10:28 AM
For certain controllers that have been switched off for a longer period of time (e.g. if they are in storage), the battery discharges and the internal time of the controller is lost if it is not connected to an NTP (Network Time Protocol) server.
Recommendations and measures:
1. If the controller is connected to an NTP server as described in the documentation, a discharged buffer battery has no negative or functional effects. The connection to an external PC can also be used as an NTP server.
2. If no NTP server is available, the invalid certificates or licences can be bypassed via a software update to version RM21.11.6. In this case, the controller continues to operate with the last valid time.
In both cases, replacing the battery is also a temporary solution.
If the reduced battery lifetime disturbs the operation, please contact Bosch Rexroth Service department.
10-14-2022 10:09 AM
Hello,
The battery problem do trouble serveral customers as I know. The time of ctrlX always need to be same with PC.
Recommendations and measures:
1. If the controller is connected to an NTP server as described in the documentation, a discharged buffer battery has no negative or functional effects. The connection to an external PC can also be used as an NTP server.
How to deploy a NTP server on external PC?
I have not find the documentation about this, can you please help me?
11-22-2022 02:29 PM