Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Wifi dongle as access point

Wifi dongle as access point

Lauri
Established Member

Hello.

There was a mention in older thread that it is possible to use wifi dongle as access point in future.

Is it possible already and if it is, how it is done? I could only get it to work as wifi client.

I use TL-WN823N adapter.

7 REPLIES 7

CodeWasi
Occasional Contributor

Hello,

Yes that is true, the USB Wifi Dongle needs a Wifi Router it can connect to. I will provide some screenshots later, but you got it already running, right?

Bye

Lauri
Established Member

Hi

I got it to work as client (picture1). But I was hoping to get it to work in the way that I could see it in my laptops wifi connections (picture2). I'm not sure if that is possible?

My goal is to take connection to CtrlX wirelessly with any laptop/panel, not only with the one that is cofigured in CtrlX Wi-Fi settings.

CodeShepherd
Community Moderator
Community Moderator

Opening a WLAN must be a feature of your stick. As far as I found the one you are using is only a client. So you cannot set up one with this hardware.

Lauri
Established Member

Ok, Thaks for reply.

Do we already have any known/tested hardware for that?

CodeWasi
Occasional Contributor

Hello Lauri,

we will release most likely the Wifi usage as Accesspoint/client by RM2207.
The handling for configuration is currently not supported by our web-ui. Manually setup with rest-api gets necessary to modify the default (client mode).

Please consider that 2 WiFi USB devices are supported right now but NOT both of them support AccessPoint-mode connected on the ctrlX.

The NETIS Wifi supports both Opmodes

CodeWasi_0-1654160010714.png

 

The TP-Link provides only client mode in connection with the ctrlX.

CodeWasi_1-1654160078655.png

Take care ording the exact type... other chipsets are not supported by the ctrlX-integrated drivers.

Bye

Open
Occasional Contributor

Hello,

Is there an updated list of Wifi dongle supported with the ctrlX? I am looking to purchase one, so i wont need to connect LAN cable to my engineering PC.

Warmest regards,

CodeShepherd
Community Moderator
Community Moderator

As far as I know no support for further adapters was added.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist