09-14-2022 02:33 AM
Hello
When I Power off and on again,I need always to Switch to Motion Operation Mode Running.
I want to know is this normal?
Solved! Go to Solution.
09-14-2022 09:11 AM - edited 09-14-2022 10:34 AM
Could you tell us which apps are installed and/or send a system report?
It could be, that you are not using an AxisProfile so the Motion will go to operational but the AxisProfile not. But this should have any effect to the function.
09-15-2022 02:13 AM
09-15-2022 07:43 AM - edited 10-17-2022 07:07 AM
Like the error indicates the AxisProfile is not booting up. So there seems to be an error there e.g. parameters mapped wrong, drive cannot be found at the EtherCat, protocol type wrong or so on.
Could you please check this topic how to switch on traces. Please choose the path "trace/rexroth-automationcore/units/comm/axisprofile" there and send an export of the logbook after the problem occurs?
10-17-2022 02:37 AM
Hi:
Please tell me how to export of the logbook after the problem occurs? Thanks.
10-17-2022 07:10 AM - edited 10-17-2022 07:11 AM
One way is to create an system report like mentioned in my post above. See the inserted link there for how to do so.
Another way way is to open the ctrlX CORE web UI and go to "Diagnostics --> Logbook" and click on the download arrow in the right top of the page.
10-20-2022 09:48 AM
Hello Sir
Do you know how to forced Switch Motion Operation Mode to Running through the program?
11-22-2022 09:59 AM
As long as there are configuration errors it will not and cannot be forced to boot up to running.