Is there a possibility to increase the accuracy of the scheduler in release 22.07?
Solved! Go to Solution.
Please consider to check the Scheduler Setup of your project.
New projects based on release RM2207 operate by default with the "Interrupt" setting of the SchedMain. In case heritage data may effect - its recommended to check the setup since the former setup with "Timer" -based do not trigger the SchedMain that precise.
As a result the Scheduler operated Task handling will benefit as well. Processes running in the context of automationcore will be handled with less jitter. Positive impact regarding F4002 - Loss of consumer connection had been feedbacked by the field - the observation was not proven, but checking the setup is recommended.