NTP time synchronisation, ctrlX CORE as a NTP server ?

NTP time synchronisation, ctrlX CORE as a NTP server ?

stefanAT_ctrlX
New Contributor

Hello,

I got following question about the NTP time sync on the ctrlX CORE: can the controller synchronize itself as an NTP client and then be available to others as an NTP server?

The system time of the ctrlX can be synchronized with a server via NTP. Can the participants in the private network then use the controller for their time synchronization?

Example:

company NTP server has IP 1.1.1.1 ;    ctrlX CORE to outside: IP 1.1.1.2 ;  to inside: 192.168.0.100

ctrlX synchronizes with 1.1.1.1 ;      participant 192.168.0.1 (private network) synchronizes with 192.168.0.100.

Regards, Stefan

1 REPLY 1

TheCodeCaptain
Community Moderator
Community Moderator

Hi st_ctrlX_user,

the ctlX CORE cannot be a NTP server.

But it could act as an router and forward the ntp requests to the outside.

To secure it a bit more you could use firewall rules to block all other traffic.

Regards

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist