FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
10-05-2022 05:00 PM
I'm using the multi-core functionality. I call within 1 Taskgroup, linked to 1 core, with different prios 4 programs. The program with the highest prio, 30, is configured with 1ms. If I check the Max. cycletime, then this value is > my configured cycle time.
Is there any way to find out, or to monitor, the cycletimes? In the past you could use a task viewer to check the task times.
Solved! Go to Solution.
10-06-2022 07:48 AM
As your seconds screenshot shows correctly only tasks can be viewed and measured not the single programs.
You could record start and end time of the programs in your application to compare it if needed.
The oscilloscope like TaskViewer was a function of the MLC that is not available for ctrlX CORE right now. But also there only tasks are visible not single programs.