12-15-2020 10:39 AM
Hi,
I have developed a Image Vision APP using OpenCV. The proble is that my core doesn't recognize the usb Webcam. Is there a list of compatible devices? i just can't get it working ☹️.
the same Cam is working fine in any other Ubuntu device with no additional driver.
To Support the OpenCV 4.0 and other Image vision/AI libraries i will need the core 20 app, can i just download it from Canonical or do i have to wait the officila Bosch release?
I kwnow that these are such difficult question but i hope there will be someone able to help me 😁
Solved! Go to Solution.
12-15-2020 01:55 PM
At the moment we only support core16 and core18 functional packges. Core20 is planned to be implement next year.
The rest is same topic like in your other post. I will post news there.
In general the ctrlX CORE can only recognize preinstalled USB devices. So there is actually a quite limited number of them also due to security reasons.