How do I reset/acknowledge faults and warnings?

How do I reset/acknowledge faults and warnings?

ctrlXnovo
New Contributor

I'm using RM21.07 system apps.  I have generated a warning and later, a fault:

ctrlXnovo_0-1628798506335.png

Previous to this warning and fault, my CORE had a solid green indicator.  Once the warning occured, it blinked green.  I had commanded an acceleration above a limit for one drive.  I corrected the error, re-issued the command with a lower than limit value and even commanded a MC_RESET on the axis.  But the warning persisted and the LED continued to blink green.  I could not find a way to make it reset to solid green.  A similar behavior occured for the fault and the LED started blinking red.  My axis was in the wrong state for the command, so I issued another reset command to clear this error.  I can then enable the axis and run it, but the LED is still blinking red.

I thought that perhaps there is a system reset in the data layer.  I cannot find a suitable command that works through the web interface.  Nor can I find a status that indicates a fault.  The fault only appears in the logbook section and there is no reset that I see or can find there either.  The only way I know to reset both the fault and warning is to reboot the control.

How do I reset the control such that the LED returns to solid green?

3 REPLIES 3

CodeShepherd
Community Moderator
Community Moderator

The error state of the ctrlX CORE is not directly connected to the motion app. so if you only reset the error in the motion the system will not recognize this.

See the pending diagnostic dialogue to see how clearing/confirming errors is done (e.g. use the developer function of your browser):

CodeShepherd_1-1628940123198.png

Or you could have a look to this topic where the error confirmation was done via the REST interface and NodeRed.

EDIT: Moved topic to ctrlX CORE.

This is my Pending Diagnostics while the LED is blinking green.  To cause the warning, I commanded an acceleration higher than the axis limit:

ctrlXnovo_0-1629122524150.png

I see no way to get back to the non-blinking, green LED status.

Then I generated an error by commanding a Jog while the axis was disabled. The LED blinks red and I have errors in the Pending Section as you describe.  The reset button is there and if I use it, the LED returns to solid green.  

How can I "reset" a warning to get back to the solid green LED?

I will check why the the warning is not visible. Normally warnings do acknowledged automatically  as soon as the reason for it gone.

To get back to solid green send following command:

 

PUT/WRITE
https://192.168.1.2/automation/api/v1.0/diagnosis/confirm/error
payload=null

 

EDIT: Actual state is visible on the Data Layer:

CodeShepherd_0-1629187034388.png

 

 

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist