01-06-2024 12:25 AM
Hello!
I have an issue with the username and password initially set up on my Ctrlx Core. Someone configured a username and password, but they don't remember that information. Now, I need to use it for a project, and I can't because I need to know those details. Is there any way to recover them? Is there a way to factory reset the Ctrlx Core to allow me to assign a new username and password? No projects have been done before, so it doesn't matter if the data is erased. I already tried with the username and password "boschrexroth," and it didn't work. Attached screenshot.
Solved! Go to Solution.
01-08-2024 09:07 AM
earch the forum, there are multiple topics which explain how to do it using an SDcard
01-08-2024 10:53 AM
Hello,
Simple you must have access on the collaboration room then you have to:
Here the file you should have in the uSD
01-09-2024 09:49 AM - edited 10-11-2024 04:35 PM
Please have a look in the online documentation "Hardware reset of the ctrlX CORE and the ctrlX DRIVE Plus with integrated ctrlX CORE".
10-11-2024 01:54 PM
Hi..
this link is not working shows blank page ... tried to refresh the page but still the same...
snapshot is attached here.
Please share the updated link..
10-11-2024 04:35 PM - edited 10-11-2024 04:35 PM