FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
06-23-2023 03:00 AM
Customer is using CtrlX Core Plus connecting to CtrlX Drive through EtherCAT as shown in picture. I did the scan device and add the drive through Ctrl IO engineering (ignoring the bus coupler of the CtrlX Core Plus). However it shows Topology Not OK.
I wonder if i miss out anything during setting up.
Solved! Go to Solution.
06-23-2023 07:31 AM
What was shown while scanning the EtherCAT? For the direct connected IOs there is an internal bus coupler that needs to be added to the fieldbus configuration as it as device that is always there and EtherCAT needs to have a complete configuration.
06-26-2023 08:55 AM
The drive is blue so it's in parametrisation or configuration mode, get in to operating mode and it might look different.
11-15-2023 09:38 AM
@Bobby Are there any news? Is this still an issue? Or can this topic be closed?