09-05-2024 06:01 PM
Hello
I am programming a PLC program with motion in CoreX-C-X3-11-ANNN-21.01-01RS-NN-NN The time since I power CoreX, booting until PLC and drive is running is 2.40 seconds
Is possible to reduce this time?
I am using a web panel WR, this panel waits 35 seconds to initialice after that WebIQ app is running but error connection is generated because Corex is still booting. After the Corex is run (2.4 seconds) I have to power off and power up webpanel again to stablishing connection betwen Corex and Web panel.
exist any other way to refresh Webpanel App when Corex begins to run?
09-06-2024 08:34 AM
Reducing the booting time is quite not possible. See also topic "Boot-Duration of real ctrlX Core X3".
For the second topic see "Workaround for delaying startup of HMI on WR panels".
09-06-2024 07:38 PM
Thanyou for your soon respond
I tryed to follow example to increase delay time in Kiosk mode, the kiosk node version in example is V1.0.17 and my version installed is V1.0.6, the webview is not available in my version, is possible to update Kiosk version from 1.0.6 to 1.0.17? do you have any procedure to do that
09-18-2024 02:57 PM
Please have a look to topic "WR21 cannot update to RC7" for how to update.