cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

CTRLX CORE Simulation on Ubuntu Machine

CTRLX CORE Simulation on Ubuntu Machine

Deniz
Member

Hello all,

I would like to run Python scripts under the ctrlx-automation-sdk without using the CtrlX Core hardware. Is it possible to simulate CtrlX device on the Ubuntu OS.

If possible, how can I implement this ? I would like to read/write data to the datalayer

Thank you
Best Regards

Deniz

3 REPLIES 3

Luschuerz
Long-established Member

If you have access to CtrlX Works it should be possible to set up a virtual CtrlX on your device. However I believe its only for windows OS so far. You can do everything with virtual CtrlX just like with a real CORE. 

 

Luschuerz_0-1644502885022.png

 

Hi,

Thanks for the reply. Yes, unfortunately ctrlx works is only available for Windows OS. Is there any other way to run virtual ctrlx core on Ubuntu OS ?

CodeShepherd
Community Moderator
Community Moderator

In general the ctrlX COREvirtual is QEMU based virtualisation. So it could also be run on a Ubuntu OS. But beware that this is not supported at the moment.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist