cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

After boot Blue light stays on

After boot Blue light stays on

AndroidzZ
New Contributor

Hello,

I had sometrouble with the ctrlX CORE. I created a clean PLC project and placed the FB IL_Ping inside of it ( i wanted to check connection to the outside), see:

AndroidzZ_0-1674038598675.png (Ip adres is of an NTP server)

After the download the response of the FB was: The remote device has not answered 

When i tried to go offline the button did not respond. The webinterface of the CORE was also not 100% responsive, for example: 

I pressed the PLC app button on the side, it opened the page but didnt show anything.

I tried to adjust some IP setting, i could change the settings but the save button didn't do anything. After a couple of more tries i Rebooted the system. Now when rebooted the core First lights up red, than flashing blue and last it stays blue. The webinterface tells met The app is curently not availible, so the core cant be reached. 

I'm gonna do i factory reset and download the program again, see if the problem reoccurs.

Anything else i might have missed or how the core could be stuck in boot? 

 

 

7 REPLIES 7

CodeShepherd
Community Moderator
Community Moderator

Please check if PLC watchdog is active so the system cannot get overloaded by not correctly working function blocks.

Further I would suggest to use the CXA_SocketComm library that is available in standard to do such stuff:

ctrlX PLC Engineering CXA_SocketComm.pngctrlX PLC Engineering CXA_SocketComm pingctrlX PLC Engineering CXA_SocketComm ping

Watchdog was active and set to 2000ms.

for the Ping Function I did use the CXA_SocketComm library

CodeWasi
Occasional Contributor

Do you mind to operate with the asynconous type..

CodeWasi_0-1674816954643.png

 

Is this still an issue or can this topic be closed?

This can be closed

Could you please share your solution with the community?

At the time factory reset seemed like the only option.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist