FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
04-22-2024 05:02 PM
Hello,
A customer wants to connect to the Symotion OPC UA server from Siemens and it is not possible to use the Browse tool. The connection is disconnected and the node tree cannot be opened. Looking at the logs shows that the limit of nodes to be read is reached.
Is there a solution for this?
Thanks
Solved! Go to Solution.
04-23-2024 07:47 AM
Please do not post the same question several times. Topic will be clarified in "Node browse error when connect Symotion via OPC UA".