cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Local Connect is in Runtime Mode, WebIQ Designer cannot be used. Error

Local Connect is in Runtime Mode, WebIQ Designer cannot be used. Error

felX_CORE
Member

Hello everyone,

 

I wanted to connect with the WebIQ Server from my core over the WebIQ Designer with the extension " --ws-host=10.52.152.57 --ws-port=10123", resulting in the error message below:

felX_CORE_1-1623833781832.png

I disabled the running HMI on the core server using the remote runtime manager and also stopped the local server on my PC without success.

 

I'm thankful for every suggestion.

Felix

1 REPLY 1

felX_CORE
Member

The Message occured because of the unfinished licencing.

With the new WebIQ Server App 2.9.2 and my installed license it works like charm.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist