10-18-2024 12:20 PM
Hello,
Is it possible to limit the number of characters (String) in an Input Field? Specifically at the time of screen input.
Thanks
Solved! Go to Solution.
10-18-2024 12:33 PM
This is only possible with a custom widget currently.
10-21-2024 09:48 AM - edited 10-21-2024 09:49 AM
The Template-for-cartesian-handling-systems-v2-6-3 includes a customer widget cx-input using a customer keypad where you can limit the input length of strings. See documentation of template for basic information of usage. Max. value of item is used as max. input length.
Therefor you either can use cx-input or create a customer widget, which open the virtual keypad by calling cxt.keypad().