cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Device Driver

Device Driver

aFouraker
Occasional Contributor

Is it possible to create an interface to read write data not using OPC-UA? For example, read/write data to a 3rd party controller? 

4 REPLIES 4

webiq-sk
Frequent Contributor

Sure, you can write your own custom IO Handler in C++ using our SDK provided - or have us create that for you.
As we love openness we use the open non-proprietary OPC-UA standard by default and usually map other proprietary or specific protocols using a custom IO Handler or using a Node.JS (JavaScript) based OPC-UA server to connect those systems like e.g. ModBus. You can download a ModBus-2-OPC-UA server for free in our customer area and of course also adapt it to your own protocols.

aFouraker
Occasional Contributor

@webiq-sk, I am not sure about that package you mentioned. That seems to need to run on my local windows machine and provide a modbus interface to opc-ua client that WEB-IQ uses. I am asking if I can add something other that OPC-UA to the application. For example, could I create a driver that will run on the web-iq server that will pull data from an allen-bradley PLC and that I can use to write data to that plc.

webiq-sk
Frequent Contributor

If you want to use a datasource in WebIQ like the OPC-UA datasource then you'd have to use a custom IO Handler written in C++ as mentioned before.

webiq-sk
Frequent Contributor
Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist