08-25-2022 07:48 AM - edited 08-25-2022 07:50 AM
Hello,
I was trying to follow the SDK quick start guide on the link below, but it says I need to download and install ctrlX Works 1.14 with function 'App Build Environment', the latest version I can find is 1.12.9. I would like to know if there is an expected release date for v 1.14? Also if there is an alternative SDK guide for the current release?
Thanks
https://boschrexroth.github.io/ctrlx-automation-sdk/quick-start-guide.html
Solved! Go to Solution.
08-25-2022 01:53 PM
Hello Tamer,
You can use the following 2 links to set up a qemu VM without App Builder Environment. (Instructions for Linux and Windows available)
https://boschrexroth.github.io/ctrlx-automation-sdk/setup_qemu_ubuntu.html
https://boschrexroth.github.io/ctrlx-automation-sdk/connecting_qemu_vm_ctrlx.html
Version 1.12 is the officially supported software release. Version 1.14 and 1.16 are not officially supported. With this in mind, if you would still like access to versions 1.14 or 1.16 for any non-real applications, we can request this permisson for you.
03-16-2023 10:55 AM
Hello,
are there any news on a release date for a new official supported software version (higher than v1.12) ?
The reason is we would like to run a real application with the PLC-Open "MC_MoveVelocity" Function Block.
It seems like the FB is already implemented in the higher versions https://docs.automation.boschrexroth.com/doc/1785661279/mc-movevelocity/latest/de/
but not officially released.
Thanks.
Max
03-16-2023 02:35 PM
Just to sum it up: