cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

build error in sdk samples-node

build error in sdk samples-node

So I got this to work once this morning on a seperate vm instance, now on this new one all build files will not work.

when running the shell script it exits with an error

 

the build-snap-amd64.sh script fails in

find: ‘/home/boschrexroth/ctrlx-automation-sdk/samples-node/datalayer.client/parts/app/install/lib/node_modules/$npm_package_name/node_modules/ctrlx-datalayer/prebuilds’: No such file or directory

Failed to run 'override-build': Exit code was 1.

Tags (1)
3 REPLIES 3
CodeShepherd
Community Moderator

Re: build error in sdk samples-node

Could you please tell us which versions of the SDK and ctrlX WORKS you did use?

Re: build error in sdk samples-node

I must have forgotten to reply to this at some point. However, I am using the latest release of the sdk on ctrlx 1.14.1 the issue is coming from an issue with using npm. I get locked up any npm install. 

npm V8.19.2
node V16.18.0 

The proccess always get stuck at idealTree:boschrexroth: sill idealTree buildDeps

This prevents any node.js build from working. becuase one or more import librarys will not exist

Now this issue exists only in the virtual build enviroment (not using an HTTP/HTTPS proxy).

 

 

CodeShepherd
Community Moderator

Re: build error in sdk samples-node

Is is this still an open issue or can the topic be closed?

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist