Reverse Proxy HTTP/HTTPS conflict

Reverse Proxy HTTP/HTTPS conflict

CtrlXplorer
Established Member

Hello everyone,

I'm encountering an issue with my Express server snap where HTTPS requests are failing when accessing the /express-server endpoint using the URL https://192.168.0.205/express-server. However, accessing https://192.168.0.205:9595/express-server works fine (see screenshots below). It's important to note that I'm not using Unix sockets and I am using a reverse proxy to port 9595 (defined in the package assets file).

Additional Info:

Build environment: Ubuntu 22.04
Snap base: core22
CtrlX CORE X3 (with core 22 app installed)
CtrlX Works version: 1.20.5

I'm using self-signed certificates to grant HTTPS access.
Additionally, when I hosted the server as HTTP, certain view elements load, but others do not due to HTTP/HTTPS conflict.

I've also observed that accessing https://192.168.0.205/express-server throws a 502 Bad Gateway error. And a message that ''The app is currently not available'' is being rendered .

At the end, my aim is to maintain HTTPS for all requests, ensuring a secure connection throughout.

Screenshots:

image1.png

image2.png

image3.png

package.assets File:

 

 

{
    "$schema": "https://json-schema.boschrexroth.com/ctrlx-automation/ctrlx-core/apps/package-manifest/package-manifest.v1.1.schema.json",
    "version": "1.0.1",
    "id": "datalayer-visualizer-app",
    "configuration": {
      "appDirectories": [
          {
              "name": "datalayer-visualizer-app",
              "description": "Datalayer Visualizer App",
              "icon": "bosch-ic-directory",
              "scopes": [],
              "copyOnLoad": true,
              "writeProtected" : false
          }
      ]
  },
    "services": {
      "proxyMapping": [
        {
          "name": "express-server.web",
          "url": "/express-server",
          "binding": ":9595",
          "options": [
            {
              "option": "websocket",
              "value": ""
            }
          ]
        }
      ]
    },
    "menus": {
      "overview": [],
      "sidebar": [
        {
          "id": "datalayer-visualizer-app-sidebar",
          "title": "Datalayer Visualizer App",
          "icon": "bosch-ic-directory",
          "link": "/express-server",
          "items": []
        }
      ],
      "settings": []

    }
  }

 

 


app.ts File:

 

 

#!/usr/bin/env node

// Import required Node.js modules
import fs from 'fs'; // File system module for handling files
import https from 'https'; // HTTPS module for creating secure servers 
import express from 'express'; // Web framework for Node.js
import cors from 'cors'; // Middleware for enabling CORS
import dotenv from 'dotenv'; // Load environment variables from .env file
import path from 'path'; // Path module for handling file paths
import cookieParser from 'cookie-parser'; // Middleware for parsing cookies

// Load environment variables from .env file
dotenv.config();

// Security: We have to trust self-signed certificates by default (ctrlX WebServer)
process.env.NODE_TLS_REJECT_UNAUTHORIZED = '0';

// Create a new express application instance
const app = express();

// Enable CORS
app.use(cors({
  origin: '*',
  methods: ['GET', 'POST', 'PUT', 'DELETE'],
  allowedHeaders: '*',
}));

// Serve static files from the public folder
app.use(express.static(path.join(__dirname, 'public')));

// Set the views directory
app.set('views', path.join(__dirname, 'views'));

// Set the view engine to EJS
app.set('view engine', 'ejs');

// Parse incoming requests with JSON payloads
app.use(express.json());

// Parse incoming requests with urlencoded payloads
app.use(express.urlencoded({ extended: false }));

// Parse incoming requests with cookies
app.use(cookieParser());

// Define a route for the root URL ('/')
app.get('/', async (req, res) => {
  // Redirect to '/express-server'
  res.redirect('/express-server');
});


// Define a route for the main page ('/express-server')
app.get('/express-server', async (req, res) => {

  // Render the main page using the EJS template
  res.render('index');
});

// Asynchronous function to start the server
async function startServer() {
  try {

    const options = { 
      key: fs.readFileSync(path.join(__dirname, 'config','key.pem')),
      cert: fs.readFileSync(path.join(__dirname, 'config','cert.pem'))
    };

    // Port to listen on (default: 9595)
    const port = process.env.PORT || 9595;

    https.createServer(options, app).listen(port, () => {
      console.log(`[Server] Server is running on https://localhost:${port}`);
    });

  } catch (error) {
    console.error('Failed to start server:', error);
  }
}

startServer();

 

 

Any insights or suggestions on how to troubleshoot and resolve this issue would be greatly appreciated.

Thank you!

Solution: Issue was resolved by switching the protocol from HTTPS to HTTP, mofifying the static file paths and creating a directory called express-server.

6 REPLIES 6

MauroRiboniMX
Contributor

Hello, 

You have to create a http server, not a https server. Our reverse proxy is able to certify automatically your app 🙂.
Just use a normal http webserver 

nickH
Community Moderator
Community Moderator

Hi @CtrlXplorer,

I agree with @MauroRiboniMX on the http/https. But there may be a second problem. Try not to use the redirect, try to use a prefix in your server-code (e.g.: "app.use('/express-server', router)"). 

CtrlXplorer
Established Member

Hi @MauroRiboniMX  and @nickH,

Thank you very much for your quick replies. I was also about to also publish an update that reverting to using the HTTP protocol resolves the issue, partially. I also removed the redirection code ( from / to /express-server).

Another issue that occured is now only the html file loads but the static files (JS/CSS) do not load. Due to MIME type errors. (please see screenshots below)

CtrlXplorer_1-1710163578018.png

--------------------------------------------------------------------------------------------------------------------------------------------------------------------------

CtrlXplorer_0-1710163454618.png

P.S. In the other webpage http://192.168.1.1:9595/express-server those MIME types are resolved correctly.

Are there additional configurations that have to be specified my express server in order to resolve these file types?



Hello, 

Yes, now you should format correctly the requests

Now you are asking files that are not present 😉 you have 2 options:
- you serve the files from a folder named expresse-server in that case they should be resolved
- you route correctly the request. 

Basically you should ask for https://192.168.1.1/express-server /stylesheets/style.css and serve the right file! You should look in the HTML file.

Thank you @MauroRiboniMX I will test one of the options that you just suggested and update you regarding the outcome. 😅

Write me if you don't suceed 😁

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist