FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
06-26-2023 03:01 PM
Hello @all,
Is there currently the possibility to integrate the datalayer as an interactive tree in an own developed webapp?
Like the ctrlX web interface, Device Bridge or even Node-Red?
--> see screenshot
Until now I only used the Datalayer Rest API to query the single nodes. Unfortunately this is not very comfortable.
Similar to DeviceBridge, I would like to browse in the datalayer tree and select individual nodes.
I would be glad about a suggestion.
Thanks!
Solved! Go to Solution.
06-26-2023 03:38 PM
Take a look at the following example: Python Datalayer Client Browse
You could modify this example to display the top level datalayer tree by default. Each time a new node is selected in the Web UI, the browse node is updated in the Python client and the discovered nodes are returned to the UI to be displayed.
06-26-2023 03:43 PM - edited 06-26-2023 03:44 PM