07-26-2024 02:05 PM
Hello,
The Cedalo Mosquitto MQTT Broker has two types of licenses: one for 110 connections and one for 1100 connections.
What does "connections" mean in this case? Does it refer to the number of MQTT clients or the number of defined topics?
Additionally, can we extend the license?
Thank you
Solved! Go to Solution.
07-31-2024 10:36 AM
From my point of view it is the number of connected clients at the same time. The Cedalo MQTT Broker counts in this way ("The number of simultaneously connected MQTT clients (devices, applications, sensors, etc.)").
Up to now there wasn't the need to extend the licenses.