05-03-2022 09:32 PM
Hello dear community members,
When I was trying to upload the SDDML (sercos description file) of the CtrlX-Drive into my IndraWorks ML 14V22 P12, I faced the Error (attached here). I had previously installed the CtrlX-Works 1.12.7.
However, after getting the SDDML files from the CtrlX-Works version 1.14.1, I was able to succesfully upload the files into the same IW.
Are there any plans to fix the SDDML files in the CtrlX-Works 1.12.7 DeviceDatasheet folder?
Thanks a lot!
Solved! Go to Solution.
05-18-2022 12:32 PM
I did send a request to integrate the fixed SDDML files to the next Patch of ctrlX WORKS 1.12. But actually ther is no timeschedule available for the next Patch.