01-11-2023 12:15 AM
Hello,
Do you have example how We can read / write Acyclicaly parameters on ctrlX Drive with Profinet with MLC Profinet FBs ?
Thanks!
Solved! Go to Solution.
02-07-2023 03:08 PM
Hello,
which version of ctrlX Drive firmware are you using?
03-06-2023 03:32 PM
acyclic access via
- SIP TCP/IP protocol, details https://docs.automation.boschrexroth.com/doc/699034151/s-ip-protocol/latest/en/
- Profinet Read / Write Record with the help of the Alias Parameters is possible with at least AXS-V-0316 or newer (AXS-V-0314 support access to I&M only)
Example Siemens PLC available, SIP function works with ctrlX Drive and IndraDrive.
https://www.boschrexroth.com/de/de/search.html?q=tia&lang=DE&origin=header&num=10&s=download