FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
05-15-2024 09:33 AM
Hello,
On my machine, I have Indracontrol L25 (Motion-PLC) in running state. IP address 192.168.1.100.
I lost backup program file due to hard disk crash of my laptop. I have software IndraWorks ML* 14V22 P10 copy.
I wish to upload program from this Indracontrol L25 and then I want to see running program online.
Can i do this ?
Warm Regards,
Satish.
Solved! Go to Solution.
05-15-2024 03:29 PM
A project archive can be stored on the CF card via FTP when archiving a project. This must be consciously activated via checkbox ff. And if the project is later restored from there, and the compiler information and the IW version at the time of creation match the data in the controller, then you can also log in or be online directly.
Conclusion: The project must first be stored on the controller (CF card).