04-08-2024 06:45 PM
Hello All,
I have had an issue occasionally with indraworks, where I am working on a winstudio project, and I need to add a variable to the OPC UA list, and when I do it doesnt create an application variable. Most of the time where I drag process variabels into my OPC UA list, it automatically creates an applicaton variable with the same name.
I've encountered this at least 10 times, the solution is never the same or i would not be asking this right now.
When it happens I basically get stuck and cant add the variables that I want to add. Its like my Application variabels list goes crazy, and I delete stuff or add stuff, but it always either comes back or goes away, and ultimately never gains communication with the new variable I've added.
Curious if anyone else has encountered this, and perhaps come up with a best solution.
Thanks
05-06-2024 09:13 AM
Hello,
it is a strange behavior. Some ideas we have:
the license does not match the amount of used tags
the tag exists already
the tag name is not valid
for a detailed investigation we need the project to have a look upon
Peter
09-05-2024 11:06 AM
Are there any news? Can this topic be closed?