Ethercat in HCS01

Ethercat in HCS01

David08
Long-established Member

Hello,

I am testing with a CtrlX starter Kit version 1.4 and would like to use the Ethercat Master with the HCS01 firmware 20.

I have configured the Drive as a slave to Ethercat SoE, and I have added in the CtrlX I/O repository the thercat xml for CS control cards.

CtrlX I/O recognizes the Drive when scanning the devices, but then an error occurs when passing OP.

David08_0-1601470409580.png

Could you tell me the necessary configuration of ethercat for a HCS01.

Thanks in advance.

7 REPLIES 7

PedroReboredo
Community Moderator
Community Moderator

Moved to ctrlX WORKS (IO Studio).

stefanAT_ctrlX
New Contributor

Did you use the function Search for devices ?

st_ctrlX_user_0-1601477216623.png

Regards, Stefan

 

David08
Long-established Member

Hello,

Yes,:

David08_0-1601478549827.png

Is the default configuration valid? Is it necessary to modify any parameter?

David08_1-1601478669513.png

David08_2-1601478687010.png

Thanks.

 

CodeWasi
Occasional Contributor

Hello David08,

could you please try the setting just changing the Distributed-Clock to freerun-mode.

Return to you tomorrow.

Bye Jens

David08
Long-established Member

Hello Jens,

With the freerun-mode configuration and a Load Basic Parameters, the Drive already works with Ethercat correctly.

Thank you very much for the help.

CodeWasi
Occasional Contributor

Hello David08,

I just scanned scanned a ID with MPB20V and active ECAT-interface with IOEng from release ctrlXWorks-package 07/20 and the scan worked fine. the default settings with Distr.Clocks setup run instantly. No modifications had been necessary. Please compare your setup on the Ecat-Master (I did not modify them).

Since I can not remember to reloaded a MPX description file the deployment of ctrlX-Works should contain the ones that works for me.

Bye, Jens

PS: Please check and return with your respults anyway.

David08
Long-established Member

Hello Jens,
Yes, I have tried again with the default configuration, without touching the Distr.Clocks and it works perfectly. The problem I had yesterday, I think was some parameter out of range because I didn't do a factory reset to the Drive (It was previously working with another fieldbus configuration).

Thanks for everything.

Regards David.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist