FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
01-30-2024 04:02 PM - edited 01-30-2024 04:05 PM
Hi all, i build my machines with two Rexroth drives( MPB20/21 and MPE20) via Ethercat SOE . I have a strange problem and it seems that the the Drive MPB20/21 lost the communication for some ms or this is what i think . At the video https://www.youtube.com/shorts/g7PCFLUaDUI you can see that the Values (position feedback and some others) that are inputs to my plc from the drive are going to 0 and after take values again .I have to noticed that at the second drive MPE20 all this values are Stable all the time . I appreciate any help because its very important to solve this issue.
01-30-2024 04:18 PM
Moved to corresponding sub forum "IndraWorks, IndraControl for MLC/MTX, IndraDrive".
01-31-2024 01:59 PM
What control system are you using? Did you have a look to the control system monitoring. Usually it shows if some telegrams were not received in time on a special monitoring screen e.g. at a Beckhoff control. Vice versa maybe send as well the drive parameter file (in format "all parameters"). There you should see if a communication problem F4... error is present.
01-31-2024 06:15 PM
02-01-2024 06:40 AM