FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
11-12-2023 10:31 PM
Hello again,
I am back with another IndraWorks related question. I have downloaded IndraWorks 14V22 P17 and installed the Engineering XLC variant following one of the forum colleagues advice.
The card that I have with the controller has FWA-CML65*-XLC-13V24-D0 written on it. When connecting to the XLC L65 controler I noticed I can choose between XLC14VRS and XLC13VR from the firmware version and also from the Firmware Release I chose 13V24.003 and it all worked with no issues (had to change the compiler version to 13 as it was default 14 and it didnt work when trying to login)
Since I am in the trial period, the next obvious step is to buy the software. Am I doing the right thing to buy the SWA-IWORKS-ML*-14VRS-D0-DVD or is it the wrong one?
Will it have the option to install the XLC Engineering variant when prompted. Will I be able to switch to XLC13VRS as I am now?
It's my first time working with Bosch and your advices and patience is highly appreciated.
Thank you so much,
AM
Solved! Go to Solution.
11-13-2023 07:55 AM
The mentioned "SWA-IWORKS-ML*-14VRS-D0-DVD" is only including the DVD with the software, that you can (and did) download also directly from the internet.
For licencing it is a little depending what you like to do. There is an IndraWorks license for only version 13 "R911337436 - SWLAWORKS-ML1-13VRS-DO-ENG - Single license IndraWorks Engineering (MLC, XLC, IL LV)" or a license that is version independent "R911332861 - SWL-WORKS-ML*-NNVRS-DO-ENG -Single License - IndraWorks Engineering MLC, ILC/XLC from 11VRS"
The easiest way would be to get in direct contact with your corresponding sales person to clarify your questions. You can find a contact via our homepage www.boschrexroth.de.