cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

use REST API to set axis command (i.e.:power on axis )

use REST API to set axis command (i.e.:power on axis )

giustola69
Long-established Member

Hello,

I'm having some problem to use the REST API to set an axis command: for instance the power on.

I tried to set the axis limit and it works but I'n not able to set any axis command. Maybe I use the wrong commands

I'm using Postman to set the API command ( below you have the screenshot of the succesfull command and unsuccesfull one )

Could you help me ?

Many Thanks

Giuseppe

4 REPLIES 4

CodeShepherd
Community Moderator
Community Moderator

The path you try to command to must be  the command itself and also the payload has to look different.

Path:

POST https://localhost:8443/automation/api/v1.0/motion/axs/AxisX/cmd/power

Payload:

{"value":true,"type":"bool8"}

 

There is an how to use the REST API in the blog area. Please have a look there for further hints.

Also the documentation of the ctrlX Data Layer will be improved with the new release RM21.03 ( version 1.8).

 

giustola69
Long-established Member

Hello,

I tried the power command with your advice and then I modify it as in the attached screenshot ( I set it like the limit command which is working ) but in both cases I got the same error ( see attached screenshot )

What Am I doing wrong ?

Thanks

Giuseppe

You are using a PUT command but as I mentioned in my instructions above you have to do a POST.

And please beware that you will always have to send an actual valid bearer token in the authorization header.

giustola69
Long-established Member

Hello,

Ok sorry, now it's working.

Many Thanks

Giuseppe

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist